Cubemars - 17 Year Motor Manufacturer info@cubemars.com +86 13755649079
English
English
中文简体
日本語
Deutsch
Français
한국어
Español
Pусский
Quick Registration
Create your CubeMars account

 

Moment
TABLE OF CONTENTS
What Is an Exoskeleton Actuator?
Definition of an Exoskeleton Actuator
What Components Make Up an Exoskeleton Actuator?
Main Types of Exoskeleton Actuators
Key Technical Characteristics of Exoskeleton Actuators
Why Are Exoskeleton Actuators Increasingly Emphasizing High Power Density?
Why Do Exoskeleton Actuators Have Higher Requirements Than Ordinary Robot Motors?
Core Design Objectives of Exoskeleton Actuators
Why High Power Density Is Extremely Important for Exoskeleton Actuators
In-Depth Analysis of CubeMars Actuator Exoskeleton Application Cases
Case 1: Exoskeleton System Based on Human-Machine Interaction Force Estimation
Case 2: AI Adaptive Exoskeleton System Application
Power Density vs Human Safety: How to Balance Them?
Recommended Motor Selection Table for Exoskeleton Actuators
Conclusion

How do exoskeleton actuators balance power density and human safety?

CubeMars / May 07,2026

 With the rapid development of smart wearable devices, rehabilitation assistance, and human-machine collaborative equipment, exoskeleton actuators are becoming important core components in the field of high-end motion control.

 

Whether in assistive systems, rehabilitation devices, or load-bearing support equipment, actuators directly determine:

 

  • Output force

  • Motion sensitivity

  • Wearing comfort

  • Human interaction safety

 

However, in the field of exoskeletons, there has always been a key technical contradiction:

 

Higher power density often means greater output torque and a more compact structure; while human safety requires the actuator to possess compliance, controllability, and low-impact characteristics.

 

So, how exactly can exoskeleton actuators achieve a balance between “high performance” and “high safety”?

 

What Is an Exoskeleton Actuator?

 

An Exoskeleton Actuator is a power unit used to drive human joint movement, typically applied in:

 

  • Assistive wearable devices

  • Rehabilitation assistance systems

  • Human motion enhancement devices

  • Human-machine collaborative equipment

 

It is mainly responsible for providing human joints with:

 

  • Torque output

  • Motion assistance

  • Dynamic following

  • Motion control

 

A complete exoskeleton actuator usually consists of the following parts:

 

  • Motor

  • Reduction mechanism

  • Encoder

  •  Driver

  • Control system

 

Its function is similar to “mechanical muscles,” helping the human body achieve easier and more stable movement.

 

Definition of an Exoskeleton Actuator

 

An Exoskeleton Actuator is the core power device used to drive joint movement in an exoskeleton system, responsible for providing assistive torque, motion control, and dynamic response for human movement.

 

It is usually installed at the human body's:

 

  • Hip joint

  • Knee joint

  • Ankle joint

  • Shoulder joint

  • Arm joints

 

and other motion areas, achieving assistance and enhancement of human movement by simulating the working method of human muscles.

 

What Components Make Up an Exoskeleton Actuator?

 

A complete exoskeleton actuator usually includes:

 

  • Motor

  • Reduction mechanism

  • Encoder

  • Driver

  • Torque control system

  • Communication module

 

Some high-end actuators also integrate:

 

  • Force sensors

  • Temperature monitoring systems

  • Braking protection modules

 

forming a highly integrated all-in-one joint drive unit.

 

Main Types of Exoskeleton Actuators

 

1. Medical Rehabilitation Exoskeletons

Help patients with stroke, spinal cord injuries, and similar conditions recover walking and movement abilities.

 

2. Industrial Assistive Exoskeletons

Used for high-intensity work such as handling and assembly to reduce worker fatigue and occupational injuries.

 

3. Military/Enhanced Exoskeletons

Enhance human load-bearing capacity, endurance, and operational efficiency.

 

Key Technical Characteristics of Exoskeleton Actuators

 

As the core power unit of the entire system, exoskeleton actuators not only determine the upper limit of output capability, but also directly affect the naturalness of human-machine interaction and the long-term wearing experience. As application scenarios continue to expand from industrial assistance and rehabilitation training to complex human-machine collaboration, their technical requirements are also continuously increasing.

 

At the design level, exoskeleton actuators are no longer merely components that “provide power,” but comprehensive systems that must simultaneously satisfy high-performance output, human safety control, and compliant interaction experience. Therefore, their key technical characteristics have gradually evolved around multiple core dimensions.

 

Technical CategoryCore ContentTechnical Key PointsValue Brought
High power densitySmall size with high output capabilityHigh slot fill rate design / High-performance permanent magnet materials / Compact structureLighter weight, stronger output, easier to wear
Precise torque control“Force”-centered control methodHigh-precision current control / Real-time torque feedback / High-bandwidth systemsMore natural movement and smoother human-machine collaboration
Compliance and backdrivabilityImprove the naturalness of human-machine interactionLow inertia design / Low friction structure / Compliant control algorithmsReduce stiffness and improve movement comfort
High safety controlHuman safety-first mechanismTorque limitation / Current protection / Temperature monitoring / Emergency stop mechanismsPrevent overload and accidental injury
Low inertia and fast responseRapidly follow human movementLow inertia motors / High-speed current loops / High-response driversSmoother gait and more synchronized movements
Highly integrated designIntegrated joint structureIntegration of motor + driver + encoder + sensorsMore compact structure and higher reliability
Thermal management capabilityGuarantee for long-term stable operationHeat dissipation structure optimization / Temperature monitoring / Current limiting controlImprove endurance and wearing comfort
Intelligent human-machine collaborationFuture development directionGait prediction / Motion recognition / Adaptive controlSmarter and more natural assistance experience

 

Overall, the technological development of exoskeleton actuators has gradually shifted from single “output capability optimization” toward a comprehensive balanced design of “performance + safety + human experience.”

 

Among them, the relationship between high power density, compliant control, and human safety is particularly critical, as they jointly determine whether the actuator can truly adapt to long-term wearing and complex human-machine interaction scenarios.

 

Why Are Exoskeleton Actuators Increasingly Emphasizing High Power Density?

 

The reason exoskeleton actuators are becoming increasingly sensitive to “high power density” is not simply the pursuit of stronger output, but is fundamentally determined by their application target (the human body) and usage method (long-term close-fitting wear).

 

Compared with ordinary robot motors, exoskeleton actuators must simultaneously satisfy the triple constraints of “power performance + human safety + wearing experience,” making power density a core indicator that determines the success or failure of the system.

 

Why Do Exoskeleton Actuators Have Higher Requirements Than Ordinary Robot Motors?


Ordinary robot motors are usually used in fixed environments, such as:

 

  • Industrial robotic arms

  • Automated production line equipment

  • Fixed trajectory motion systems

 

The characteristics of these scenarios are:

 

  • No need for close-fitting wear

  • Do not directly act on the human body

  • Allow relatively large weight and volume

  • Place more emphasis on stable output and lifespan

 

However, exoskeleton actuators are completely different, as they are directly attached to the human body, and their operating environment is “human.”

 

This brings three fundamental differences:

 

Core ConstraintSpecific RequirementAffected AreaMain ImpactDesign Orientation
Must be worn close to the body (extremely high weight sensitivity)Actuators are installed at joint areas (knees / hips / ankles)Lower limb and upper limb jointsAlters gait, increases energy consumption, accelerates fatigueMake the system as lightweight as possible while ensuring output capability
Must coexist with humans (cannot use rigid driving)Follow human movement, avoid interfering with natural motion, and prevent forced pullingWhole-body motion chainAffects movement naturalness and interaction experienceImprove compliance, reduce impedance, and enhance natural interaction
Must operate for long periods (sensitive to heat and comfort)Long-term wearing, low temperature rise operation, stable outputEntire wearable systemAffects comfort and continuous usage experienceOptimize heat dissipation and energy efficiency to ensure long-term stable operation

 

Core Design Objectives of Exoskeleton Actuators


The design of exoskeleton actuators is not simply about pursuing “greater power” or “higher speed,” but about achieving a comprehensive balance between power output and interaction experience under human-body constraints. Since they directly act on human joints, the design objectives must simultaneously consider performance, safety, and long-term wearing experience.

 

Overall, the core design objectives of exoskeleton actuators can be summarized in the following aspects:

 

Design ObjectiveCore PositioningCore RequirementsEssential Goal
High power densityFundamental performance objectiveDeliver greater torque output within a smaller volume; reduce joint burden; improve structural compactnessAchieve stronger power output with a lighter structure
Compliant controlHuman-machine interaction objectiveDynamically adjust output according to human movement; smooth torque transitions; avoid rigid impactsAllow the device to “follow the human” instead of “control the human”
Human safetySystem constraint objectiveDual torque and current limitations; abnormal protection mechanisms; safe motion range control; real-time temperature and load monitoringEnsure no uncontrollable risk is caused to the human body under any circumstances
BackdrivabilityNatural movement objectiveReduce mechanical impedance; reduce friction sensation; improve passive following capabilityAllow the human body to naturally drive actuator movement
Wearing comfortLong-term use objectiveLow weight burden; low heat output; stable continuous operation; reduced fatigue accumulationAchieve comfortable long-term wearing without affecting daily movement


Why High Power Density Is Extremely Important for Exoskeleton Actuators

 

In the design of exoskeleton actuators, high power density is not only a performance indicator, but also a key factor that determines whether the system is “usable, easy to use, and suitable for long-term use.” It directly affects weight control, power output, human safety, and the overall wearing experience, making it one of the core constraints of the entire system design.

 

From the perspective of practical applications, the importance of high power density is mainly reflected in the following aspects:

 

Key FunctionCore IssueImpact of Insufficient Power DensityImprovements Brought by High Power Density
Solve the contradiction between lightweight design and output capabilitySimultaneously require “strong output + light weight”Larger motor size, increased weight, increased burden on the human bodyAchieve greater power output in a smaller and lighter structure
Reduce the burden of human wearingJoint positions are extremely sensitive to weight (knee/hip/ankle)Heavier equipment, increased motion inertia, increased energy consumption, easy fatigueReduce single-joint load and overall energy consumption
Improve compliant control and movement naturalnessNeed smooth human-machine collaborative movementLarge inertia, slow response, stiff movementLower inertia, faster response, smoother torque output
Improve human safety boundariesHuman movement control in dynamic environmentsSlow response, high impact risk, control lagFast closed-loop control to reduce impact and loss-of-control risks
Improve backdrivability and natural interaction experienceThe human body needs to naturally drive the actuatorHigh resistance, strong mechanical sensation, unsmooth movementReduce system impedance and improve natural following capability
Improve long-term wearing comfortRequirement for long-term close-fitting operationHeavy joint burden, rapid fatigue accumulation, poor experienceLighter, more energy-efficient, and more comfortable continuous usage experience

 

The reason why high power density has become a core indicator of exoskeleton actuators is essentially not a single performance improvement, but because it simultaneously solves:

 

●  Power output capability

●  Human load control

●  Movement naturalness

●  Safety response capability

●  Long-term wearing experience

 

Therefore, it is more like a “system-level balance indicator,” directly determining whether exoskeleton actuators can truly achieve:

 

The unified experience of lightweight design + high output + compliant control + human safety + comfortable wearing.

 

In-Depth Analysis of CubeMars Actuator Exoskeleton Application Cases


Case 1: Exoskeleton System Based on Human-Machine Interaction Force Estimation


 qdd-based-hri-force-estimation


Project Background

 

In human-machine collaborative exoskeleton systems, “interaction force” is a key parameter affecting control accuracy and wearing comfort. Traditional solutions usually rely on additional force sensors to measure the interaction force between humans and machines, but this approach brings obvious problems:

 

  • Increased system weight

  • Higher overall cost

  • Increased structural complexity

  • Reduced integration reliability


Therefore, the industry has begun exploring a lighter and more efficient solution: achieving precise human-machine interaction force estimation without adding extra sensors.


CubeMars Actuator Solution

 

This project uses CubeMars actuators to build a hip-joint exoskeleton system, realizing interaction force estimation through the dynamic characteristics of the actuator itself.

 

The core design relies on the following key capabilities:

 

Technical CapabilityFunction
High power densityProvide sufficient joint assistance while reducing overall system weight
Compliant control capabilityAchieve more natural human-machine interaction and force feedback
Low mechanical impedanceReduce movement resistance and improve human active control capability
High response performanceImprove control accuracy under dynamic changes


Project Results

 

During treadmill walking experiments, test subjects performed movement tests under different assistive torque conditions.

The system demonstrated the following results:

 

  • Average error controlled within a relatively low range

  • Significantly improved torque tracking accuracy

  • Enhanced human-machine interaction stability

 

This indicates:

 

Even without additional force sensors, high-precision human-machine interaction force estimation can still be achieved.


Technical Significance

 

The core value of this case lies in verifying that:

 

Through the intrinsic characteristics of high-performance actuators, system structure can be simplified while simultaneously improving control accuracy.

 

At the same time, it performed outstandingly in the following aspects:

 

  • Improve human safety (reduce sudden impacts)

  • Enhance compliant control capability (more natural movement)

  • Optimize backdrivability (smoother human movement)

  • Improve wearing comfort (reduce long-term fatigue)


Case 2: AI Adaptive Exoskeleton System Application


 validation-II-real-world-community-walking


Project Background

 

With the development of artificial intelligence and motion control technologies, exoskeleton systems are evolving from fixed assistance modes toward adaptive intelligent control.

This project was jointly developed by multiple universities, with the goal of achieving:

 

  • Complex terrain adaptation

  • Real-time gait recognition

  • Dynamic assistance adjustment

  • Long-term natural wearing experience

 

This places higher requirements on actuators.


CubeMars Actuator Solution

 

The system adopts CubeMars actuators as the core drive unit to support complex dynamic motion control.

Its key technical support includes:

 

Technical CapabilityFunction
High power densityProvide stable power output while ensuring lightweight design
Compliant control capabilityAchieve natural collaborative movement between humans and machines
High backdrivabilityImprove the freedom of human active movement
Low mechanical impedanceReduce the “mechanical feeling” of movement and improve natural experience
High dynamic responseRapidly adapt to gait changes and environmental changes


Project Results

 

The system can automatically adjust assistance strategies according to different motion scenarios, including:

 

  • Walking on flat ground

  • Going up and down stairs

  • Uphill and downhill movement

  • Gait speed switching

 

During dynamic changes, the actuator can rapidly respond to changes in human movement, effectively reducing:

 

  • Sense of movement delay

  • Mechanical dragging sensation

  • Gait coordination problems


The overall movement performance becomes smoother and more natural.


Technical Significance

 

This case verifies the core role of exoskeleton actuators in intelligent control systems:

 

Actuators are not only the source of power, but also the key determining factor of the human-machine interaction experience.

 

Its core value is reflected in:

 

  • Improve human safety boundaries (reduce impact risks)

  • Enhance compliant control capability (more natural movement)

  • Optimize backdrivability (easier human-driven movement)

  • Improve wearing comfort (suitable for long-term use)

  • Support stable output under high power density

 

Through the above two cases, it can be seen that the development of exoskeleton actuators no longer simply relies on “greater output,” but is gradually shifting toward:

 

  • Power density (lightweight + strong output)

  • Compliant control (natural human-machine interaction)

  • Human safety (system bottom-line constraints)

  • Backdrivability (movement naturalness)

  • Wearing comfort (long-term usage experience)

 

This also shows:

 

The core value of exoskeleton actuators is not to “drive human movement,” but to “allow humans to move more naturally.”


Power Density vs Human Safety: How to Balance Them?


In exoskeleton actuators, motors not only determine the power performance of the equipment, but also directly affect human safety and the wearing experience. Therefore, compared with simply pursuing higher power, human safety has always been the most important core factor in exoskeleton actuator design.

 

Although high power density can make exoskeleton actuators lighter, more compact, and provide stronger assistance effects, excessively high output capability may also bring:

 

  • Excessive movement impact

  • Uneven joint force distribution

  • Unstable control

  • Unsynchronized human-machine movement

 

Since exoskeleton actuators are devices that directly act closely on human joints, once the motor output loses control or the response becomes unnatural, it may affect human joints, muscles, and even overall movement balance. Therefore, exoskeleton actuators not only need to be “powerful,” but also “safe, stable, and controllable.”


How to Improve Human Safety?

 

In order to ensure safety under high power density conditions, modern exoskeleton actuators usually adopt the following control and design strategies:

 

  • Torque control: Make output softer and more natural, avoiding rigid driving

  • Impedance control: Reduce mechanical impact and improve movement smoothness

  • Torque limiting protection: Prevent excessive output under abnormal conditions from causing injury

  • Low inertia design: Improve response speed and movement stability

 

The core goal of these strategies is:

 

While ensuring power output capability, make human-machine interaction more controllable and natural.


Why Is High Power Density Still Necessary?

 

High power density remains a key development direction for exoskeleton actuators because it directly affects:

 

  • Lightweight structural design

  • Assistive output capability

  • Compliant control performance

  • Backdrivability and natural movement experience

  • Long-term wearing comfort

 

In other words, high power density determines “how powerful the system can be,” while safety control determines “whether it can be used stably.”


Core Logic of Balance

 

In exoskeleton actuator design, the relationship between the two can be summarized as:

 

Power density determines the upper performance limit, while human safety determines the application boundary.

 

A truly excellent solution is not about choosing between the two, but about fully releasing performance while ensuring safety.


The design objective of exoskeleton actuators is not simply to pursue higher output capability, but to achieve a system-level balance among:

 

  • Power output

  • Control accuracy

  • Human safety

  • Wearing comfort

 

thereby achieving a truly sustainable long-term human-machine collaborative experience.

 

Recommended Motor Selection Table for Exoskeleton Actuators

 

In exoskeleton actuator systems, different joint positions (hips, knees, ankles, etc.) and different application scenarios have very different requirements for motor performance. During selection, the following key factors usually need to be comprehensively evaluated:

 

  • Power density

  • Torque output capability

  • Human safety

  • Overall weight

  • Control accuracy

  • Compliant control capability (Backdrivability)

 

Among them, high power density and compliant control capability are becoming the core trends in exoskeleton actuator motor selection, ensuring that the system is both “powerful” and “lightweight and safe.”

 

ModelRecommended ApplicationCore FeaturesApplicable Area
AK10-9 V3.0 KV60High-load exoskeletons / Lower-limb assistive systemsHigh torque output, high power density, dual-encoder structureHip joint / Knee joint
AK80-9 V3.0 KV100AI intelligent exoskeletons / Gait assistive systemsHigh response speed, low mechanical impedance, strong compliant control capabilityKnee joint / Ankle joint
AK80-6 KV100Lightweight exoskeleton systemsHigh integration, lightweight, stable operationLower-limb assistive structures
AK70-10 KV100Industrial assistive exoskeletonsHigh torque load capacity, strong impact resistanceHip joint
AK60-6 V3.0 KV80Portable exoskeleton devicesMiniaturized design, high efficiency, low inertiaAnkle joint / Small assistive modules
AKE SeriesRehabilitation and augmentation exoskeleton systemsHigh compliance control, excellent backdrivability, natural human-machine interactionLower-limb joint systems


Recommended Selection Directions (By Application Scenario)


Application ScenarioRecommended Motor DirectionKey Requirements
Medical rehabilitation exoskeletonsHigh compliance control + high-precision controlHuman safety priority, natural movement
Industrial handling exoskeletonsHigh torque + high stabilityLong-duration continuous output, load resistance
AI intelligent exoskeletonsHigh response + high-bandwidth controlDynamic gait recognition and real-time adjustment
Lightweight wearable devicesHigh power density + miniaturized designReduce human burden and improve comfort


Conclusion


With the development of robotics technology, AI control algorithms, and high-performance actuators, exoskeleton actuators are gradually moving from laboratories into practical application scenarios such as medical rehabilitation, industrial assistance, and intelligent wearables. As the core power source of the system, actuator selection and performance directly determine overall experience, safety, and usability.


1. Exoskeleton actuators not only determine power performance but also affect human safety and wearing experience:Unlike traditional industrial motors, exoskeleton actuators directly interact with human joints for long periods, so they emphasize compliant control, human-machine collaboration, and long-term comfort in addition to output capability.


2. High power density is an important development direction for exoskeleton actuators:Higher power density means achieving stronger assistive output within smaller size and lighter weight, helping improve flexibility, reduce human burden, and optimize overall system integration.


3. Human safety always takes priority over extreme power output:Since exoskeleton actuators directly interact with human joints, their design must ensure safety boundaries through low mechanical impedance, torque limiting protection, compliant control, and related capabilities to avoid rigid impacts and motion imbalance.


4. Compliant control and backdrivability are the key foundations of human-machine collaboration:Excellent exoskeleton actuators should not only “provide power” but also “adapt to human movement.” By reducing impedance and improving backdrivability, the human body can naturally drive the system, creating a smoother interaction experience.


5. Future development direction: lighter, smarter, and safer:With advancements in AI control algorithms and highly integrated actuator technologies, exoskeleton actuators will continue evolving toward higher power density, greater control precision, and more natural human-machine interaction, further enhancing real-world application value and commercialization potential.


The development of exoskeleton actuators is shifting from “simply pursuing power performance” toward a system-level balance of “power density, control precision, safety, and human experience.”


In the future, achieving a better integration between high-performance output and human safety will become the key to advancing exoskeleton technology toward mature real-world applications.

Related Articles
How Highly Integrated Robotic Actuators Enable Superior Robot Motion
How Highly Integrated Robotic Actuators Enable Superior Robot Motion
Highly integrated robotic actuator solutions enhance precision and response speed, reduce system latency, and enable high-performance motion for humanoid and industrial robots.
Apr 08,2026
How to Choose the Right Robot Joint Motor: Torque, Speed & Integration Explained
How to Choose the Right Robot Joint Motor: Torque, Speed & Integration Explained
Learn how to select the right robot joint motor by analyzing torque requirements, speed, and precision to ensure stable, efficient, and reliable robotic motion.
Feb 10,2026
Torque motor, How does it work?
Torque motor, How does it work?
Torque motors are a type of electric motor that is designed to provide high levels of torque or rotational force. They are commonly used in applications where precise control of motion is required, such as robotics, medical equipment, industrial machinery
Sep 11,2023
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt